This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133 Load design for 3 Cell testing

Other Parts Discussed in Thread: BQ24133

BQ24133 is used for designing Li-ion Battery charger for 3 cell. The battery voltage is available as 12.6V at output.

I don't have a testing circuit for constant current load as mentioned in the testing evaluation guide.

The input voltage, VIN is 15V

The observations without load are:

SRP = 1.21V, SRN=1.21V, AVCC= 14.96, TS=2.97V, OVPSET= 1.379V, ACSET= 1.054V, ISET= 0.2745V, REGN = 6V, BATDRV = 15.26V,

CELL= VREF= 3.3V,

Please provide a load circuit or any alternative to test the charging before connection the battery.