Other Parts Discussed in Thread: TPS84620
Hello,
In my design I'm using a TPS84620 to produce 2.5V and I want to make sure I get the resistor and cap settings correct.
On Table 1 it shows for 2.5V that Rrt should be set 1K ohm while Table 2. says it should be open, which is correct?
On Table 3 it says to use a minimum of 200uF on the output of the power supply but on Table 4 it shows a configuration that is only 147uF, which is correct?
Is there any significant difference between running with two separate grounds for agnd and pgnd vs just having one single ground?
Thank you,
John Kasson