This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090 Error Writing Configuration

Other Parts Discussed in Thread: UCD9090

We have a new design that uses the UCD9090 sequencer and out of the 7 prototype boards that I have tried to program so far, 3 of them are giving the same error.  The exact error that I am getting from the Fusion Digital Power Designer software is:

There was an error writing your project file's configuration to the device:
wrote 15 of 358 parameters from the project file (343 errors), but could not save the device configuration to flash: STORE_DEFAULT_ALL sendbyte on UCD9090 @ Address 65d error: NACK

The exact sequence of steps I am using to attempt to program the device are:

  1. Connect the USB Interface Adapter to the UCD9090.
  2. Power on the board.
  3. Open the Fusion Digital Power Designer.
    1. It correctly identifies and connects to the UCD9090.
    2. Since the device on this board has never been programmed, the software tells me I don't have any rails defined and asks me what to do.
  4. I select "Import a device configuration from a project file" and click Next.
  5. I select the project file that we have developed and successfully used with at least 4 other boards and click Next.
  6. During the write to the device, there are a massive number of errors in the Error Log.
  7. When I click Next, I am presented with the error message given above.

I have tried the above steps multiple times on each of the boards that have failed and get the same results each time.  Now, given that this is a new design, I can't rule out the possibility of a hardware issue, so I'm really looking for ways to try to troubleshoot this problem.

  • What are the first a few errors?
    I would check I2C waveform first to rule out signal integrity issue.
  • I assume you mean from the error log?  They are:

    SEQ_CONFIG [Rail #4] write Rail On Dep: Rail #1,6,7 | GPI On Dep: <None> | Rail Off Dep: Rail #5 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,5,6,7,8,10 | Enable: Pin 17 FPWM8_GPIO12 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x3E00000000000061001002F6] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #5] write Rail On Dep: Rail #1,2,3,4,7,10 | GPI On Dep: V | Rail Off Dep: Rail #8 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,6,7,8,10 | Enable: Pin 24 GPIO15 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0xA60800000000024F008002EE] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #6] write Rail On Dep: Rail #1,7 | GPI On Dep: <None> | Rail Off Dep: Rail #2,3,4 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,7,8,10 | Enable: Pin 13 FPWM4_GPIO8 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x1E00000000000041000E02DE] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #7] write Rail On Dep: Rail #1,10 | GPI On Dep: V | Rail Off Dep: Rail #4,5,6 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,8,10 | Enable: Pin 12 FPWM3_GPIO7 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x1608000000000201003802BE] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #8] write Rail On Dep: Rail #1,5,7 | GPI On Dep: V | Rail Off Dep: Rail #9 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,7,10 | Enable: Pin 11 FPWM2_GPIO6 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x0E080000000000510100027E] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #9] write Rail On Dep: <None> | GPI On Dep: <None> | Rail Off Dep: <None> | GPI Off Dep: <None> | Fault Dep: Rail #1,2,3,4,5,6,7,8,10 | Enable: Unassigned; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x0400000000000000000002FF] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #10] write Rail On Dep: Rail #1 | GPI On Dep: <None> | Rail Off Dep: Rail #4,5,7 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,7,8 | Enable: Pin 10 FPWM1_GPIO5 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x0600000000000001005800FE] on UCD9090 @ Address 65d error: NACK

    The entire log is attached here.

    Write Log:
    
    Starting write of 358 parameters ...
    Wrote VOUT_MODE [Rail #1] EXP -12 [0x14] to RAM
    Wrote VOUT_MODE [Rail #2] EXP -12 [0x14] to RAM
    Wrote VOUT_MODE [Rail #3] EXP -13 [0x13] to RAM
    Wrote VOUT_MODE [Rail #4] EXP -13 [0x13] to RAM
    Wrote VOUT_MODE [Rail #5] EXP -13 [0x13] to RAM
    Wrote VOUT_MODE [Rail #6] EXP -14 [0x12] to RAM
    Wrote VOUT_MODE [Rail #7] EXP -14 [0x12] to RAM
    Wrote VOUT_MODE [Rail #8] EXP -14 [0x12] to RAM
    Wrote VOUT_MODE [Rail #9] EXP -10 [0x16] to RAM
    Wrote VOUT_MODE [Rail #10] EXP -14 [0x12] to RAM
    Wrote MONITOR_CONFIG [MFR 05] Pin 1 MON1: Not Assigned; Pin 2 MON2: Rail #8, Type Voltage; Pin 38 MON3: Rail #5, Type Voltage; Pin 39 MON4: Not Assigned; Pin 40 MON5: Rail #4, Type Voltage; Pin 41 MON6: Rail #3, Type Voltage; Pin 42 MON7: Rail #7, Type Voltage; Pin 45 MON8: Rail #9, Type Voltage; Pin 46 MON9: Rail #6, Type Voltage; Pin 48 MON10: Rail #1, Type Voltage; Pin 37 MON11: Rail #2, Type Voltage [0x0027240023222628252021] to RAM
    Wrote GPI_CONFIG [MFR 41] Inputs: Pin 26 GPIO17 ActiveLow Input,Pin 21 GPIO14 ActiveHigh Input,Pin 15 FPWM6_GPIO10 ActiveHigh Input,Pin 25 GPIO16 ActiveHigh Input,Pin 7 GPIO4 ActiveHigh Input,Pin 4 GPIO1 ActiveHigh Input [0xB1552DAD957D00000000000000] to RAM
    Wrote SEQ_CONFIG [MFR 38,Rail #1] Rail On Dep: <None> | GPI On Dep: <None> | Rail Off Dep: <None> | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,7,8,9,10 | Enable: Unassigned; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x5400000000000000000003FE] to RAM
    Wrote SEQ_CONFIG [MFR 38,Rail #2] Rail On Dep: Rail #1,6,7 | GPI On Dep: <None> | Rail Off Dep: Rail #5 | GPI Off Dep: <None> | Fault Dep: Rail #3,4,5,6,7,8,10 | Enable: Pin 16 FPWM7_GPIO11 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x3600000000000061001002FC] to RAM
    Wrote SEQ_CONFIG [MFR 38,Rail #3] Rail On Dep: Rail #1,6,7 | GPI On Dep: <None> | Rail Off Dep: Rail #5 | GPI Off Dep: <None> | Fault Dep: Rail #2,4,5,6,7,8,10 | Enable: Pin 14 FPWM5_GPIO9 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x2600000000000061001002FA] to RAM
    Saving device configuration (RAM) to flash memory ...
    
    Error Log:
    
    SEQ_CONFIG [Rail #4] write Rail On Dep: Rail #1,6,7 | GPI On Dep: <None> | Rail Off Dep: Rail #5 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,5,6,7,8,10 | Enable: Pin 17 FPWM8_GPIO12 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x3E00000000000061001002F6] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #5] write Rail On Dep: Rail #1,2,3,4,7,10 | GPI On Dep: V | Rail Off Dep: Rail #8 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,6,7,8,10 | Enable: Pin 24 GPIO15 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0xA60800000000024F008002EE] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #6] write Rail On Dep: Rail #1,7 | GPI On Dep: <None> | Rail Off Dep: Rail #2,3,4 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,7,8,10 | Enable: Pin 13 FPWM4_GPIO8 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x1E00000000000041000E02DE] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #7] write Rail On Dep: Rail #1,10 | GPI On Dep: V | Rail Off Dep: Rail #4,5,6 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,8,10 | Enable: Pin 12 FPWM3_GPIO7 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x1608000000000201003802BE] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #8] write Rail On Dep: Rail #1,5,7 | GPI On Dep: V | Rail Off Dep: Rail #9 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,7,10 | Enable: Pin 11 FPWM2_GPIO6 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x0E080000000000510100027E] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #9] write Rail On Dep: <None> | GPI On Dep: <None> | Rail Off Dep: <None> | GPI Off Dep: <None> | Fault Dep: Rail #1,2,3,4,5,6,7,8,10 | Enable: Unassigned; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x0400000000000000000002FF] on UCD9090 @ Address 65d error: NACK
    SEQ_CONFIG [Rail #10] write Rail On Dep: Rail #1 | GPI On Dep: <None> | Rail Off Dep: Rail #4,5,7 | GPI Off Dep: <None> | Fault Dep: Rail #2,3,4,5,6,7,8 | Enable: Pin 10 FPWM1_GPIO5 ActiveHigh ActivelyDrivenOutput; Seq On Timeout: 0 / Wait Indefinitely; Seq Off Timeout: 0 / Wait Indefinitely [0x0600000000000001005800FE] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 0; [0x00] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 1; [0x01] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 2; [0x02] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 3; [0x03] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 4; [0x04] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 5; [0x05] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 6; [0x06] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 7; [0x07] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_INDEX write GPO Index 8; [0x08] on UCD9090 @ Address 65d error: NACK
    GPO_CONFIG_10 write Unassigned; No Mask [0x000000000000000000000000000000000000000000] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 0 [0x00] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 1 [0x01] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 2 [0x02] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 3 [0x03] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 4 [0x04] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 5 [0x05] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 6 [0x06] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 7 [0x07] on UCD9090 @ Address 65d error: NACK
    PWM_SELECT write 8 [0x08] on UCD9090 @ Address 65d error: NACK
    PWM_CONFIG_9 write Pin_ID = 9; Duty Cycle: 0.0 %; Frequency: 0 Hz; Phase: 0.0 deg [0x8800000000000000] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #1] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #2] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #3] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #4] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #5] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #6] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #7] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #8] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #9] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    MARGIN_CONFIG [Rail #10] write Mode: Disabled; Increase Duty Cycle decreases Voltage; Ignore Faults: False; PWM Pin: ID 0, # 10 FPWM1_GPIO5 [0x00] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 0 [0x00] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 1 [0x01] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 2 [0x02] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 3 [0x03] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 4 [0x04] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 5 [0x05] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 6 [0x06] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 7 [0x07] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 8 [0x08] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 9 [0x09] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 10 [0x0A] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 11 [0x0B] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 12 [0x0C] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 13 [0x0D] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 14 [0x0E] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 15 [0x0F] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 16 [0x10] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 17 [0x11] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 18 [0x12] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 19 [0x13] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 20 [0x14] on UCD9090 @ Address 65d error: NACK
    GPIO_SELECT write 21 [0x15] on UCD9090 @ Address 65d error: NACK
    GPIO_CONFIG_22 write Enable: False; Out_Enable: False; Out_Value: False; Status: True [0x08] on UCD9090 @ Address 65d error: NACK
    LOGGED_FAULT_DETAIL_ENABLES write Common: LOG_NOT_EMPTY,RESEQUENCE_ERROR,RESERVED4,RESERVED5,RESERVED6,RESERVED7; GPI: #1,2,3,4,5,6,7,8; Rail #1: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #2: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #3: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #4: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #5: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #6: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #7: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #8: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #9: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT; Rail #10: VOUT_OV,VOUT_UV,SEQ_ON_TIMEOUT,SEQ_OFF_TIMEOUT [0xF5FFC3C3C3C3C3C3C3C3C3C3] on UCD9090 @ Address 65d error: NACK
    MFR_DATE write YYMMDD [0x59594D4D4444] on UCD9090 @ Address 65d error: NACK
    MFR_ID write MFR_ID [0x4D46525F4944] on UCD9090 @ Address 65d error: NACK
    MFR_LOCATION write MFR_LOCATION [0x4D46525F4C4F434154494F4E] on UCD9090 @ Address 65d error: NACK
    MFR_MODEL write MFR_MODEL [0x4D46525F4D4F44454C] on UCD9090 @ Address 65d error: NACK
    MFR_REVISION write MFR_REVISION [0x4D46525F5245564953494F4E] on UCD9090 @ Address 65d error: NACK
    MFR_SERIAL write 000000 [0x303030303030] on UCD9090 @ Address 65d error: NACK
    MISC_CONFIG write Time Between Resequences: 1024 msec; Resequence Abort: no; Max Resequences: 2; FIFO Mode: All; Brownout Enable: yes [0x1790] on UCD9090 @ Address 65d error: NACK
    PIN_SELECTED_RAIL_STATES write State 0: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 1: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 2: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 3: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 4: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 5: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 6: Enabled=No, Turn Off Mode=ImmediateOff, Rails States= ; State 7: Enabled=No, Turn Off Mode=ImmediateOff, Rails States=  [0x000000000000000000000000000000000000] on UCD9090 @ Address 65d error: NACK
    RESET_COUNT write 0  [0x0000] on UCD9090 @ Address 65d error: NACK
    RUN_TIME_CLOCK_TRIM write -0.66 % [0xB560] on UCD9090 @ Address 65d error: NACK
    SECURITY_BIT_MASK write No commands write protected [0x0000000000000000000000000000000000000000000000000000000000000000] on UCD9090 @ Address 65d error: NACK
    SYSTEM_RESET_CONFIG write Disabled [0x000000000000000000] on UCD9090 @ Address 65d error: NACK
    SYSTEM_WATCHDOG_CONFIG write Disabled [0x00000000] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #1] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #1] write Retry Time: 0 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A [0x000000000000000000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #1] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #1] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #1] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #1] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #1] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #1] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #1] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #1] write 4.250 V [0x4400] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #1] write 4.500 V [0x4800] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #1] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #1] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #1] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #1] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #1] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #1] write <No Limit> [0x8000] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #1] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #1] write 5.000 V [0x5000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #1] write 5.500 V [0x5800] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #1] write 4.500 V [0x4800] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #1] write 5.750 V [0x5C00] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #1] write 5.500 V [0x5800] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #1] write 0.435  [0xAB7B] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #1] write 4.250 V [0x4400] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #1] write 4.500 V [0x4800] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #2] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #2] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #2] write Retry Time: 960 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0x8080000000A08F0000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #2] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #2] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #2] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #2] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #2] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #2] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #2] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #2] write 2.805 V [0x2CE1] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #2] write 2.970 V [0x2F85] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #2] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #2] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #2] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #2] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #2] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #2] write 100.0 ms [0xEB20] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #2] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #2] write 3.300 V [0x34CD] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #2] write 3.465 V [0x3771] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #2] write 3.135 V [0x3229] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #2] write 3.795 V [0x3CB8] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #2] write 3.630 V [0x3A14] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #2] write 0.680  [0xB2B8] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #2] write 2.805 V [0x2CE1] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #2] write 2.970 V [0x2F85] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #3] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #3] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #3] write Retry Time: 0 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0x8080000000A0000000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #3] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #3] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #3] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #3] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #3] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #3] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #3] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #3] write 2.125 V [0x4400] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #3] write 2.250 V [0x4800] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #3] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #3] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #3] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #3] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #3] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #3] write 100.0 ms [0xEB20] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #3] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #3] write 2.500 V [0x5000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #3] write 2.625 V [0x5400] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #3] write 2.375 V [0x4C00] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #3] write 2.875 V [0x5C00] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #3] write 2.750 V [0x5800] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #3] write 0.752  [0xB302] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #3] write 2.125 V [0x4400] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #3] write 2.250 V [0x4800] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #4] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #4] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #4] write Retry Time: 960 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0x8080000000A08F0000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #4] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #4] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #4] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #4] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #4] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #4] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #4] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #4] write 1.530 V [0x30F6] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #4] write 1.620 V [0x33D7] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #4] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #4] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #4] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #4] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #4] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #4] write 100.0 ms [0xEB20] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #4] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #4] write 1.800 V [0x399A] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #4] write 1.890 V [0x3C7B] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #4] write 1.710 V [0x36B8] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #4] write 2.070 V [0x423D] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #4] write 1.980 V [0x3F5C] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #4] write 1.000  [0xBA00] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #4] write 1.530 V [0x30F6] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #4] write 1.620 V [0x33D7] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #5] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #5] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #5] write Retry Time: 0 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0x8080000000A0000000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #5] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #5] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #5] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #5] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #5] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #5] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #5] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #5] write 1.275 V [0x28CD] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #5] write 1.350 V [0x2B33] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #5] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #5] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #5] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #5] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #5] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #5] write 100.0 ms [0xEB20] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #5] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #5] write 1.500 V [0x3000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #5] write 1.575 V [0x3266] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #5] write 1.425 V [0x2D9A] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #5] write 1.725 V [0x3733] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #5] write 1.650 V [0x34CD] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #5] write 1.000  [0xBA00] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #5] write 1.275 V [0x28CD] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #5] write 1.350 V [0x2B33] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #6] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #6] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #6] write Retry Time: 0 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0x8080000000A0000000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #6] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #6] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #6] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #6] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #6] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #6] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #6] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #6] write 1.020 V [0x4148] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #6] write 1.080 V [0x451F] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #6] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #6] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #6] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #6] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #6] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #6] write 100.0 ms [0xEB20] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #6] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #6] write 1.200 V [0x4CCD] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #6] write 1.260 V [0x50A4] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #6] write 1.140 V [0x48F6] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #6] write 1.380 V [0x5852] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #6] write 1.320 V [0x547B] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #6] write 1.000  [0xBA00] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #6] write 1.020 V [0x4148] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #6] write 1.080 V [0x451F] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #7] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #7] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #7] write Retry Time: 960 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0x8080000000A08F0000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #7] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #7] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #7] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #7] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #7] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #7] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #7] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #7] write 0.850 V [0x3666] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #7] write 0.900 V [0x399A] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #7] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #7] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #7] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #7] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #7] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #7] write 100.0 ms [0xEB20] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #7] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #7] write 1.000 V [0x4000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #7] write 1.050 V [0x4333] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #7] write 0.950 V [0x3CCD] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #7] write 1.150 V [0x499A] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #7] write 1.100 V [0x4666] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #7] write 1.000  [0xBA00] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #7] write 0.850 V [0x3666] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #7] write 0.900 V [0x399A] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #8] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #8] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #8] write Retry Time: 96 msec| Max Volt Glitch Time: 100.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Enabled; Response: Shut down immediately; Restart: Do not restart| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down immediately; Restart: Do not restart| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Shut down with delay; Restart: Do not restart [0xC080000000A04CFA00] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #8] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #8] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #8] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #8] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #8] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #8] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #8] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #8] write 0.638 V [0x28D5] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #8] write 0.675 V [0x2B33] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #8] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #8] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #8] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #8] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #8] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #8] write 99.9 ms [0xEB1F] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #8] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #8] write 0.750 V [0x3000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #8] write 0.788 V [0x326F] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #8] write 0.712 V [0x2D91] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #8] write 0.862 V [0x372B] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #8] write 0.825 V [0x34CD] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #8] write 1.000  [0xBA00] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #8] write 0.638 V [0x28D5] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #8] write 0.675 V [0x2B33] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #9] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #9] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #9] write Retry Time: 0 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A [0x000000000000000000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #9] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #9] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #9] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #9] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #9] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #9] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #9] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #9] write 10.200 V [0x28CD] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #9] write 10.800 V [0x2B33] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #9] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #9] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #9] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #9] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #9] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #9] write <No Limit> [0x8000] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #9] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #9] write 12.000 V [0x3000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #9] write 12.600 V [0x3266] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #9] write 11.400 V [0x2D9A] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #9] write 13.800 V [0x3733] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #9] write 13.200 V [0x34CD] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #9] write 0.162  [0xA298] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #9] write 10.200 V [0x28CD] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #9] write 10.800 V [0x2B33] on UCD9090 @ Address 65d error: NACK
    OPERATION [Rail #10] write Unit: ImmediateOff; Margin: None [0x00] on UCD9090 @ Address 65d error: NACK
    ON_OFF_CONFIG [Rail #10] write Mode: Always Converting [0x00] on UCD9090 @ Address 65d error: NACK
    FAULT_RESPONSES [Rail #10] write Retry Time: 0 msec| Max Volt Glitch Time: 0.0 msec| Max Other Glitch Time: 0 msec| VOUT_OV: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| VOUT_UV: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_OC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| IOUT_UC: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| OT: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A| TON_MAX: Resequence: Disabled; Glitch filter: Disabled; Response: Ignore; Restart: N/A [0x000000000000000000] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_GAIN [Rail #10] write 10.0 mΩ [0xD280] on UCD9090 @ Address 65d error: NACK
    IOUT_CAL_OFFSET [Rail #10] write 0.000000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_FAULT_LIMIT [Rail #10] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_OC_WARN_LIMIT [Rail #10] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    IOUT_UC_FAULT_LIMIT [Rail #10] write 0.000 A [0x8000] on UCD9090 @ Address 65d error: NACK
    OT_FAULT_LIMIT [Rail #10] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    OT_WARN_LIMIT [Rail #10] write 255 °C [0xF3FC] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_OFF [Rail #10] write 0.850 V [0x3666] on UCD9090 @ Address 65d error: NACK
    POWER_GOOD_ON [Rail #10] write 0.900 V [0x399A] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_GAIN [Rail #10] write 100.0 °C/V [0xEB20] on UCD9090 @ Address 65d error: NACK
    TEMPERATURE_CAL_OFFSET [Rail #10] write 0.00 °C [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_DELAY [Rail #10] write 0.0 ms [0x8000] on UCD9090 @ Address 65d error: NACK
    TOFF_MAX_WARN_LIMIT [Rail #10] write <No Limit> [0x7FFF] on UCD9090 @ Address 65d error: NACK
    TON_DELAY [Rail #10] write 2.0 ms [0xBBFF] on UCD9090 @ Address 65d error: NACK
    TON_MAX_FAULT_LIMIT [Rail #10] write <No Limit> [0x8000] on UCD9090 @ Address 65d error: NACK
    VOUT_CAL_MONITOR [Rail #10] write 0.000 V [0x0000] on UCD9090 @ Address 65d error: NACK
    VOUT_COMMAND [Rail #10] write 1.000 V [0x4000] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_HIGH [Rail #10] write 1.117 V [0x477D] on UCD9090 @ Address 65d error: NACK
    VOUT_MARGIN_LOW [Rail #10] write 0.950 V [0x3CCD] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_FAULT_LIMIT [Rail #10] write 1.125 V [0x4800] on UCD9090 @ Address 65d error: NACK
    VOUT_OV_WARN_LIMIT [Rail #10] write 1.117 V [0x477D] on UCD9090 @ Address 65d error: NACK
    VOUT_SCALE_MONITOR [Rail #10] write 1.000  [0xBA00] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_FAULT_LIMIT [Rail #10] write 0.850 V [0x3666] on UCD9090 @ Address 65d error: NACK
    VOUT_UV_WARN_LIMIT [Rail #10] write 0.900 V [0x399A] on UCD9090 @ Address 65d error: NACK

  • It looks like after writing SEQ_CONFIG [MFR 38,Rail #3], all communication is lost. Are the errors the same every time?

    I would check power and I2C signal first (Is logic high high enough? Is logic low low enough?). Are there other devices on the same bus that can corrupt the communication?

    If you re-open Fusion GUI immediately after the programming failure, can GUI detect the device at the same address?
  • Yes, the errors appear to be the same each time.

    I connected an oscilloscope to the PMBUS_CLK (pin 8), PMBUS_DATA (pin 9), and power supply to the device.  The power supply voltage is always maintained between 3.2 and 3.3V.  During normal communication, the CLK and DATA signals appear to be toggling between the expected levels (0-0.1V low and 3.2-3.3V high).  What I did notice however, is that when the failure occurs, the high levels of the CLK and DATA signals decays from ~3.3V down to ~0.1V over a period of 1.5-2.0ms.  This occurs after about 150ms of "good" communication.

    If I re-open the GUI, it cannot detect any devices until I cycle power to my board.

  • I didn't mention this earlier, but we also have the I2C port of a C6674 DSP connected to the sequencer (in parallel to the USB-TO-GPIO adapter) so that we can perform updates in the field. I have found that if I disconnect the DSP, I am able to successfully program the sequencer on each of the boards that previously failed. Clearly something about the I2C connection from the C6674 DSP is improperly pulling down these signals on some of our boards, but not all of them. At the point that this is happening, the DSP isn't even out of reset because its power supplies have not come up yet.
  • Glad you have found the problem. UCD9090 will not hold down CLK for more than 35ms as it is the max allowed by PMBus standard.
  • I am wondering if there is a recommended way to connect both the USB-TO-GPIO adapter and a separate I2C master, like we are trying to do with the C6674? I'd like to try to avoid having jumpers or something of that sort, if at all possible.