I have 5V coming in, then through a Schottky, so the regulator sees about 4.7V and is very steady. Then as an RC filter at EN gets to about 1V, VIN starts to oscillate between 4.7V and 2V, and VOUT jumps to 2V. This goes on for 25ms to 100ms, at which point VIN spikes to 8V for about 500us as VOUT goes to 3.3V, then everything settles out, with VIN remaining at 4.7V.
Why the spike, and what to do about it? It's not coming from the source, and there's nothing else in the circuit. I have many boards that work, but 2 boards where the regulator appears to have died (input DC resistance is now about 150 ohms when off, and 0V on VOUT when powered). The absolute maximum rating of LM3671 VIN is 6V.
Our board only consumes about 300mA, and the design is good for at least 600mA.
Thanks,
- Tones