This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14020 fsw=2.2MHz Setting

Other Parts Discussed in Thread: LMR14020

Hi,

My customer has questions about LMR14020.
Could you tell us about questions?

[Question]
 My customer consider the design of LMR14020 fsw=2.2MHz under the following conditions. My customer has questions.

 <conditions>
 Vin=9V to 14V
 Vout=3.3V
 Iout=1.5A
 fsw=2.2MHz
 Cout=ceramic capacitor

 - How much is the value recommended of L and Cout? My customer will use ceramic capacitor for Cout.
 - How much is the accuracy of fsw?
 - Do you have a table of L, Cout and Cff typical values like the LM4360x?
 - What the switching frequency is the best for the internal compensation?

Best Regards,
tateo