Hi,
I’m using the LM5060 as a power switch and want to use the OVP feature to protect the device I am controlling the power supply to.
I have a question on the behaviour of the OVP feature as follows:
- If the supply to VIN is set so that OVP will be no higher than 1.76V, when the EN pin is set high the FET is enhanced and turns on.
- If the supply to VIN is set so that OVP is higher than 1.76V but below 2V, when the EN pin is set high the FET does not turn on.
If I am reading the datasheet correctly then the OVP feature should only work when the OVP pin is higher than 2V. So why am I seeing this behaviour?
Interestingly if I place an oscilloscope probe on the OVP net then the FET does turn on in the second instance. If the oscilloscope probe is already on the OVP net and the power is applied, the FET does not turn on.
Once the FET is on, OVP behaves as it should i.e. bring OVP past 2V and the FET turns off, bring it below 1.76V and it turns on again.
I have tried this with a few different LM5060 devices and the effect is the same.