This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Charger IC for LiFePO4 battery pack using bq76920 and bq78350?

Other Parts Discussed in Thread: BQ76920, BQ78350, BQ24620, BQ40Z60

We are designing a new LiIon battery pack for which we will need to also design a charger.

The pack will use 3 LiFePO4 cells in series. There will be 3 of these series strings in parallel. Each cell is a 3.3Ah, 3.2V nominal with a standard charge current of 0.2C. This means a pack nominal voltage of 9.6V. This chemistry and cell capacity being chosen in anticipation of meeting ATEX explosive atmosphere requirements.

Our initial selection of AFE is the bq76920 and Battery Management Controller Companion chip bq78350.

Since this chip set includes features for charging balancing and gas gauge, what IC would best suit incorporation into the charger for this pack?