Hello
I use TPS61175 for a boost converter from 12V to 24V(800mA). The maximum of input supply is 3A.
During the power on, the inupt supply is drop to 5V, and the current is about 3A . After 3~4 seconds , it's recover to normal.The input back to 12V about 2A.
Can you give me advice to solve this problem?
Thank you for your help,
Best Regards,
carry