This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3407MY/NOPB

Other Parts Discussed in Thread: LM3407

hello,

I am projecting a led driver 350mA using the 

LM3407MY/NOPB

By webench I have project it, it's a 24Vdc power supply, with  2 Osram led 3.1V 350mA.

I am testing it, but it is right up to 16Vdc, from 16 Vdc to 24 Vdc I see the light is very low. 

Is righ to use the LM3407 in this condictions? because, I see on Webench, also by flowchart, it will work right, but really it is not.

Can someone help me?

Thanks

Henry