This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

My question is reg this Gate Driver IC : UCC27527 .

Other Parts Discussed in Thread: UCC27527, UCC27528

 I intend to use  RCD for generating a Dead Time , approx 4.35 uSec. My question is regarding its Inputs , whether they can accept the slow moving Inputs that are created by the Capacitor charging of the RCD , or is there any Input current peaking as in seen in many CMOS Ckts .

Typical values may be 1.5 nF , 2.9 K Resistor shunted by a Diode .

Lastly is this IC available only in SON package or SOIC version is also either available or is being planned ?

Thanks & Regards