I make a circuit calculated with Wbench using LM3150. I decide to use a syncro platform to improve performance and reduce heating.
The only thing that i change is the MOSFETs
The circuit work, the output is 10V with an imput over the 14.5V, under this the output decrease a bit and under 13.0V the device enter in security mode, output switch on and off.
Also, it difficultly get 1A, it work good under 0,5A. All device are very cold.
I'd like that my DC DC converter gets a current of 2.5A limited vith an output of 10V with an imput from 10.5-11V to 15V.
Thank you for help.