Balancing starts when directly charging after discharging, without waiting for an OCV Measurement.
Min Rsoc for Balancing is set to 80%, but it already starts balancing at a lower Rsoc. I am Using the bq40z50-R1 Firmware!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Balancing starts when directly charging after discharging, without waiting for an OCV Measurement.
Min Rsoc for Balancing is set to 80%, but it already starts balancing at a lower Rsoc. I am Using the bq40z50-R1 Firmware!
This forum does not allow me to upload the srec file. May I send it to you via mail?
The Min RSOC for Balancing parameter only applies to balancing during Rest. The gauge will balance cells at lower SOC when in Charge mode.The IT gauges only use capacity balancing, although there is a correlation to the cell voltages. We would need to see the capacities for each cell to verify imbalance.
There was an imbalance of almost 100mV, but no OCV measurement was taken, so this imbalance was not cleared.Balancing bei 100mV Im Rest Mode erfolglos.log
I made another measurement over night. Balancing 13.log
I am using a low threshold mosfet (DMN2004DWK-7). This should be mentions somewhere in the technical Reference of bq40z50.
as I can see balancing started, but did not finish. So cells are still unbalanced.
I will run another cycle to see if it is still the case after another Qmax update and OCV measurement.
As I use three parallel 82 Ohm resistors as a balancing resistor, I am balancing with a 27Ohm resistor. so the calculated Cell Balancing times are: 80 and 81 seconds. I doubled them because I had to adjust current measurement (dividing by 2).
Roman,
I reviewed the log file and the balancing times are set properly. Note the DOD points and the balancing times. The larger the DOD value, the shorter the balancing time. Note that the DOD point for Cell 1 is the largest value and this indicates that it was the lowest voltage cell when the DOD point was set. The balancing time should be set to 0 for the highest DOD point and it is in your log file. The log file does not show when the DOD points were set, but the cell voltages for Cells 1, 3 and 4 were fairly close at the beginning of the log. It looks like Cell 4 may be damaged, because the cell voltage increases significantly as compared to the other during charging. This would indicate that the series resistance is higher. It does not look like Cell 2 is charging, so It may be damaged as well.
Tom