Hi everyone at TI and forum users,
I have been looking with many semiconductor manufacturers for a "smart" load switch(es) that can handle the following requirements:
First One:
VIN: 12V nominal (probably more like 8V < Vin < 17V)
Output current: 5A
Short Circuit Protection: something in the range of 20A - 40A
Overvoltage protection (voltage clamp): 45V or around
Overtemperature protection: when the device reaches certain temperature (for example 140°C) it can shutdown and restart automatically after the temperature has drop to certain level.
ESD protection: Human body model,
CMOS, TTL compatible (controllable from a 5V MCU)
Second One:
VIN: 5V nominal (probably more like 4.75V < Vin < 5.25V)
Output current: 3A
Short Circuit Protection: something in the range of 8A - 20A
Overvoltage protection (voltage clamp): 45V or around
Overtemperature protection: when the device reaches certain temperature (for example 140°C) it can shutdown and restart automatically after the temperature has drop to certain level.
ESD protection: Human body model,
CMOS, TTL compatible (controllable from a 5V MCU)
I am looking for output protection devices that can handle the voltage and current requirements and that have the protections stated (short-circuit, over-voltage, overtemperature, ESD). I am open to any suggestions since I have not been able to find anything suitable in the TI product range, but maybe my search has not been good.
If any experts from TI have any recommendation that match or more or less match the requirements I am willing to hear them.
Thanks!