Other Parts Discussed in Thread: TPS62170
Dear all.
TPS62170 Vref accuracy typical is 0.8V writen by datasheet.
Do you have min/max parameter?
Parametrics:
Vref Accuracy(Typ)(%) is 3%
Is this the meaning to +/-3%? or +/-1.5%?
EVM;
Output Voltage PWM Mode of Operation 3.227/3.327/3.427 V
Is this a Vref accuracy? or output? full load?
Regards,
PAN-M