This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REQUIRED BOOST CONTROLLER IC

Other Parts Discussed in Thread: TPS40210, LM5121

Hii..

I am need of a boost controller IC which is capable for the below mentioned spec.

Vin(min)             -  12V

Vin(max)            -  36V

Vout                    -  65V

Iout                     - 5.5A

Fsw                   -  525KHz.

Kindly suggest a chip. Pls do the needful.

Waiting for your valuable reply. An immediate reply is always appreciated.


Regards,

Prajeesh
.