Hello,
we have a trouble with BQ51025. We have our own design of the wireless power. We use BQ500215 as transmitter and BQ51025 as receiver. Component BQ51025 is destroyed during testing wireless power.
When we put receiver coil on the transmiter coil for the first time, it worked correctly. When the distance between transmiter's coil and receiver's coil was slowly increased, receiver BQ51025 stop to work. There are higher peaks at the receiver coils when are both coils slowly removed.
Only green LED between RECT and /WPG at the BQ51025 pins is blinking after restart the Transmitter.
Transmiter is powered to 12 VDC. Receiver has two posibilities output power 5V, 1A -> 5W or 10V, 1A -> 10W.
For three times we have destroyed BQ51025. Do you have any advice how fix it?
Your sincerely,
Tom