This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62065 - EVM (SLVU364–March 2010) layout questions

Other Parts Discussed in Thread: TPS62085, TPS82085

Dear TI,

Few questions regarding the EVM layout:

(1) The PCB stack-up is not clear. Is layer 2 close to the Top layer?

(2) Why there is a GND opening under the DC-DC in Layer 1?

(3) Why GND to FB resistor is connected thru net to AGND pin? (and not thru GND plane)

Thanks,

Igal

  • 1. Yes, layer 2 is the next one under the top layer. Figure 15 should be labeled layer 3. It's a 4 layer board.

    2. I believe this is Figure 15, which is really the 3rd layer in the PCB. This simply provides a GND flood to tie all those vias together. It's not needed.

    3. It is recommended to route the FB divider directly back to the AGND pin to eliminate any noise impacts from affecting that critical signal.

    You might look at the TPS62085 or TPS82085 as higher power, newer converters.
  • Hi Chris,

    Thanks for the answers.

    Regarding item 3 - it is not clear why AGND (to FB) is routed as a separated net in Bottom layer, while pin 3 is connected both to GND paddle and the GND via near this pin is connected to GND plane in Layer 2. Please advice?

    Thanks,

    Igal

  • Layer 2 is AGND, so the vias can tie there with no issue. If that GND plane were connected to the input and output headers as well, I would not recommending connecting the GND vias to the plane.