Helloo....
Please suggest an LDO for the below mentioned spec.
Required Vout - 14.5V
Input Range - 16V - 36V (Input voltage will fall to 12V for 30sec, During this time device should give at least 12V output)
Output current - 100mA
Package - SOIC / SOT / DPAK.
Kindly suggest a part which can achieve the spec as mentioned above. Pls do the needful at the earliest. Its urgent.
Regards,
Prajeesh