Hello,
I am implementing bq51050b for a proof of concept project, and I had a few questions about the suggested component values for various pins, and other generl questions.
- the datasheet says that capacitive communication is the "most common" - why is that? why does the EVM use resistive communication despite this? what are the tradeoffs? Also, how is the value is 47nF (as per datasheet) or 22nF (as per EVM) chosen for the COMM pin? if I were to switch to resistive communication, how would I choose the value?
- for clamping capacitors a value of 0.47uF is recommended - why is that?
- caps connected at the RECT pin are recommended to 10.1uF - why is that?
- the minimum charging current per datasheet is 500mA. what happens when the resistors are set for a charging current lower than this? will it not function or default to 500mA?
- the procedure to calibrate Rfod and Ros seems to require at least a few iterations of design, which i do not have the time for in my project schedule. how can i make a best estimate for these values (if possible)? for now i have values recommended by the datasheet as a starting point - will i run into serious errors with this setup? the inductance of my coil is roughly the same as the inductance assumed by the examples in the datasheet.
Thanks,
John