This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About over discharged battery and bq25100H

Guru 19645 points

When I make them connect the battery which did over discharge, it can't charge any more.

Is there a measure?

 

When battery protection IC connects the battery which becomes Cut-Off and supplies 5V, over discharge turns on FET for protection,

and starts to see the battery voltage, but a charge isn't done.

Therefore 5V is connected, a battery consumes an electric current, and battery protection detects over discharge, and disable again.

When 5V is turned OFF→ON before a device detects over discharge, it was charge.

 

【Additional Information】

・Battery protection IC:S-8211CDO-I6T1U (SII)  

  S-8211C web

 

  S-8211C datasheet

 

・VBAT is less than 3.3V.

 (Customer think that the battery remain is less than 5%.)

・A charge is suspended perfectly.

 →The current of the 5V power line was 0mA~1mA.  

 →When they'll be left alone, the battery voltage becomes off once again by over discharge.

 

Best regards,

Satoshi