Hi,
I'm designing a power supply with the following features:
Vin: 20V~30V
Vout: -80V
First, my choice was between the flyback and the negative boost (usign buck) topologies, but I read the application SLUA288 (Dual Output Boost Converter) and I saw there a way to generate a capacitively coupled auxiliary output, which in most of case is a negative output.
Comparing this approach to other topologies above (flyback and negative boost), it seems to be the simplest one.
Using the webench tool, I came to the circuit above:
So my question is: would the -80V work if a derive a capacitively coupled auxiliary output?
Regards,
João P. B. Figueiredo