Hi,
I have a board with a bq40z60 circuit copied from the evaluation module. When I look at the discharge current value on bqStudio, I see values that are consistently about 65% higher than what I measure with an ammeter. However, it does return the correct pack voltage.
The board has the 0.005 ohm sense resistor (R43) between SRP and SRN. And two 100 ohm filtering resistors (R38 and R44 in the EVM).
What should I be checking (hardware and data flash) to isolate the problem?
Thanks,
Charley