A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ40z50 opens charge FET on charge termination even though CHGIN bit is zero.
Other Parts Discussed in Thread: BQ40Z50I'm working with the BQ40z50 guage, and I want the charge FETS to remain on even when the pack is at 100% charge. According to the technical reference manual, setting CHGIN in Fet Options to zero will keep the FETs on after Valid Charge Termination, but my pack already has the CHGIN bit set to zero and the pack still turns off when charge terminates.
The TCA bit is a flag that is set by the 40z50, not a configuration bit to set. Is there a way to disable the TCA while still letting the pack fully charge?