I am using the BQ40Z60EVM to charge 2 series Li-ion NCR18650B. I have completed the learning cycle; max error updated to 1%, update status changed to 6, and qmax updated. Even still the gauging is not working. SOC shows 100% regardless of actual charge. I have attached a .log file of a brief charge. Please let me know if there are any settings that are incorrect.
Tue Aug 18 19:32:50 CDT 2015 Device Name = bq40z60 Firmware Version = V0_13_BLD0019 Design Capacity = 3350 Design Voltage = 7200 Specification Info = 0x0031 Manufacturer Date = 1980-1-1 Serial Number = 0x0001 Manufacturer Name = Texas Instruments Device Name = bq40z60 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,TurboPwr,TurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,ChgrStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,Vacp,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,CBTime1,CBTime2,CBTime3,CBTime4,SOH_FC_Q,SOH_FC_E,ChgVoltReg,ChgCurrReg,LogRowTime(ms),LogStatus 1,2015-08-18 19:32:54,4.152,0x0397,300,10,0x6001,0,65535,65535,1,26.8,7278,1690,1644,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3640,3639,0,0,7328,19191,1691,1690,0,0,616,615,0,0,1230,1194,35.0,26.8,26.8,27.2,27.2,26.8,35.0,23,15,0,0,23,15,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,49,12274,12290,0,0,-23,-15,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-23,0,1.56,2114,0,0,0,0,0,0,253,41,942,SUCCESS 2,2015-08-18 19:32:58,8.144,0x0397,300,10,0x6001,0,65535,65535,1,26.9,7281,1690,1655,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3642,3640,0,0,7330,19185,1692,1690,0,0,616,615,0,0,1231,1203,35.2,27.0,27.0,27.5,27.4,27.0,35.2,25,17,0,0,25,17,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,53,12274,12290,0,0,-25,-17,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-25,0,1.56,2114,0,0,0,0,0,0,253,41,944,SUCCESS 3,2015-08-18 19:33:02,12.139,0x0397,300,10,0x6001,0,65535,65535,1,27.1,7283,1690,1663,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3643,3641,0,0,7333,19185,1689,1690,0,0,615,615,0,0,1231,1210,35.5,27.1,27.1,27.6,27.6,27.1,35.5,27,18,0,0,27,18,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,57,12274,12290,0,0,-27,-18,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-27,0,1.56,2114,0,0,0,0,0,0,253,41,943,SUCCESS 4,2015-08-18 19:33:06,16.147,0x0397,300,10,0x6001,0,65535,65535,1,27.2,7286,1690,1670,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3644,3643,0,0,7334,19185,1690,1689,0,0,616,615,0,0,1232,1215,35.7,27.3,27.4,27.8,27.7,27.2,35.7,28,19,0,0,28,19,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,61,12274,12290,0,0,-29,-20,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-29,0,1.56,2114,0,0,0,0,0,0,253,41,944,SUCCESS 5,2015-08-18 19:33:10,20.141,0x0397,300,10,0x6001,0,65535,65535,1,27.4,7288,1690,1674,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3645,3644,0,0,7338,19184,1690,1689,0,0,616,615,0,0,1232,1219,36.0,27.4,27.5,28.0,27.9,27.4,36.0,30,20,0,0,30,20,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,64,12274,12290,0,0,-30,-20,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-30,0,1.56,2114,0,0,0,0,0,0,253,41,943,SUCCESS 6,2015-08-18 19:33:14,24.150,0x0397,300,10,0x6001,0,65535,65535,1,27.5,7290,1689,1678,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3646,3645,0,0,7341,19187,1691,1688,0,0,617,615,0,0,1232,1222,36.2,27.5,27.6,28.1,28.0,27.5,36.1,32,22,0,0,32,22,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,69,12274,12290,0,0,-32,-22,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-32,0,1.56,2114,0,0,0,0,0,0,253,41,943,SUCCESS 7,2015-08-18 19:33:18,28.145,0x0397,300,10,0x6001,0,65535,65535,1,27.6,7293,1689,1681,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3647,3646,0,0,7342,19185,1690,1689,0,0,616,616,0,0,1233,1224,36.3,27.6,27.6,28.2,28.1,27.6,36.3,34,23,0,0,34,23,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,72,12274,12290,0,0,-34,-23,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-34,0,1.56,2114,0,0,0,0,0,0,253,41,942,SUCCESS 8,2015-08-18 19:33:22,32.153,0x0397,300,10,0x6001,0,65535,65535,1,27.6,7295,1689,1683,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3648,3647,0,0,7345,19187,1689,1689,0,0,616,616,0,0,1232,1226,36.6,27.7,27.8,28.3,28.3,27.7,36.5,36,24,0,0,36,24,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,76,12274,12290,0,0,-36,-24,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-36,0,1.56,2114,0,0,0,0,0,0,253,41,942,SUCCESS 9,2015-08-18 19:33:26,36.147,0x0397,300,10,0x6001,0,65535,65535,1,27.9,7296,1689,1684,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3649,3648,0,0,7346,19184,1688,1689,0,0,616,616,0,0,1232,1228,36.7,27.9,28.0,28.5,28.5,27.9,36.7,38,26,0,0,38,26,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,80,12274,12290,0,0,-38,-26,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-38,0,1.56,2114,0,0,0,0,0,0,253,41,943,SUCCESS 10,2015-08-18 19:33:30,40.140,0x0397,300,10,0x6001,0,65535,65535,1,28.0,7298,1689,1685,1,100,0,0,0,65535,65535,0,1625,8266,0x0080,5,-246,-369,0,0x0397,0x0000,0x10,0x0004,0x0003,0x10,0x0818,0x0438,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3650,3649,0,0,7349,19185,1690,1689,0,0,617,616,0,0,1233,1229,36.9,28.0,28.1,28.7,28.6,28.0,36.9,40,27,0,0,40,27,0,0,0,0,25.8,25.7,1000,1000,0,0,0,0,0,0,0,6,0,0,0,0,84,12274,12290,0,0,-40,-27,0,0,0,0,0,3451,3450,0,0,12274,12290,0,0,-40,0,1.56,2114,0,0,0,0,0,0,253,41,943,SUCCESS