Hi
I am using bq27530-g1 and trying to finish the learning cycle.
in the last discharge the battery get to 0% as it should after few hours the VOK is set to 0 as it should. the "update_status_0" is set to 2 as it should. but the "qen" doesnt set to 0 and always show 1.
remark - I am doing the learning cycle manually. because bqeasy doesnt appearing in the "bq evaluation sw"... and no one answer to my post on how to add it.
now I just want to solve the qen to end this learning cycle and to have a good golden file.
thanks in advanced,