Hi, I have an existing design which utilizes all 12 separate channels of the TLC5971. We have altered the Rset resistor (680R) so its close to the absolute max, and we use a heat sink on the chip. So far so good, but I'd like to get roughly twice the brightness out of each channel from the same LEDs. The leds can handle it.
I note that the TLC5971 datasheet says multiple outputs can be wired up in parallel to increase the output current.
My question is, instead of wiring up multiple outputs from the same chip, can I hook up the outputs of 2 different TLC5971's together?
If so, can I also then put two TLC5971's with the same input SCK and DATA lines to make them behave indentically, without changing our firmware?
Kind Regards