This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z45-R1 CUV Not turning back ON properly

Other Parts Discussed in Thread: BQ20Z45-R1

I am using the BQ20Z45-R1 with a Li-Ion pack setup as a 4S3P.  I currently have the CUV threshold set to 2500mV and recovery set to 3375mV.  I am experiencing the following:

-CUV threshold is reached at 2500mV and the pack shuts OFF and remains OFF

-The pack is placed on a charger which pulse charges until it detects a battery present

-The pack turns ON for a few seconds and then back OFF with each charge pulse.  The pack will not turn ON and remain ON.  It will sit in this condition for up to 30 minutes before it may turn ON and stay ON.  When measuring the cells during this condition they are around 2900mV.

Any explanation as to why the pack is turning ON and not staying ON?