The document SLUSAW3C section 12.1.1 #8 tells us we should connect power ground to device ground (analog ground) with a zero-ohm resistor or thermal pad at one point. However, for the bq40z60EVM board it seems like the PGND and GND are only connected through the sense resistor R43. Is this what I should do on my own design? If I connect PGND to GND then wouldn't R43 stop having current flow through it?