This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z60 wake command with no charger present



Everything I can find for this question seems to require we apply power to VAC first.  I desire for the circuit to be automatically powered from the moment the battery itself is connected, even if the charger is not there.  I feel this should be possible, since BAT is the primary power input and the circuit can stay on after the wake-up button is pushed without a charger being present, but I can't seem to get it to work. 

  • Voltage must be applied to VAC to wake-up the device, if it is in the shutdown state. After batteries have been attached and the device is operating, then voltage does not have to be applied to VAC to wake it up from sleep mode.