Hello,
I use a BQ24640 for charge a supercapacitor (25F) with the following setting:
Icharge=120mA => Viset = 0.82V
Vc= 2.6V.
Vin = 15V
During the design, I measure two different charge current :
Icharge = 90mA when Vc < 1.6V
Icharge = 120mA when Vc>1.6V
I not find any explanation of this comportment in the datasheet.
Are you any explain for this? (Current limitation? ...)
Best regards
Emeric