Hello,
I am currently working of project which is required 12V, 10A DC Output from the input voltage range of 8-25V... So i have refereed data-sheet of LM5175 which shows that i can get max. 6A and 12V output... It's not met my requirement ..
But when i have check with TI's Webench with passing these above parameter it will give solution with same but it shows output current 10A... It is ok for me..
My question is : Is it possible to get 10A using this design which is given by Webench ?
I have attached PDF given by Webench...webench_design_TI_12V_10A_8V_to_25V.pdf