Hi,
Does TPS65921 have any limits on the amount of current it can provide in USB500 mode? Will I be able to draw the 1.5A promised current (or 1.4A from TPS65921) when it is connected to a CDP ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does TPS65921 have any limits on the amount of current it can provide in USB500 mode? Will I be able to draw the 1.5A promised current (or 1.4A from TPS65921) when it is connected to a CDP ?
Thanks.
Muzaffer Kal I've moved your question on TPS65921 to the (DO NOT USE) PMIC Forum so that team can further assist you.