This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063A DC-DC converter for 1.2V generation

Other Parts Discussed in Thread: MC34063A, LM25085A, TPS54540

1. We are using MC34063A DC-DC converter IC for 3.3V output generation from 40Vinput, we would like to know can we generate 1.2V out put from same IC?

2. As per datasheet MC34063A can deliver maximum peak switch current of 1.5A with internal MOSFET

Currently We are using external MOSFET for driving 1.5A average current(3A peak)

but now we need output current of 2.5A average current(5A peak), our query is

Can we useexternal MOSFET of higher rating while changing current sense and Inductor to meet the requirement of 2.5 A average current?

 

 

.