Dear all,
I am designing a battery management circuit that includes a BQ24230 battery charger and a BQ27441-G1 fuel gauge.
In our design, an ON/OFF controller driven by a push-button is used to connect/disconnect the system from the battery (including the host microcontroller and its dedicated power supply). The charger is directly connected to the battery: it does not depend on the ON/OFF controller to allow battery charging even if the push-button has not been pressed.
I have the following questions:
- Is it better to keep the fuel gauge outside the system (no ON/OFF controller dependency)?
- Knowing that the GPOUT output should not be left floating, what is the best solution if I want to connect it to the host microcontroller which can be disconnected from the battery?
- Are there any other recommendations other than 1MOhm pull-downs on I2C lines in this configuration?
Thank you in advance.
Best regards.