This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5023 Error code

Dear,

      I am using 11.1V Lithium Battery in SMBUS. its charging and discharging FET are ON  but at o/p only 1.3 V is showing through multimeter and in pack voltage  calibration  5023 error code is showing. If we connect charger at its P+  P- pts. pack voltage calibration is done but as we remove supply then again it shows 5023 error code. what can be the reason behind it