Hi,
My customer is considering to use BQ24251, and I received some quesions.
Could you help to get the socket?
1-1. On the D/S fig 7 and 8, the units of IBAT are "A".
I think that these units are too large, are these correct?
1-2. Is the condition of the fig 7 the same as "Input UVLO" of Fault condition?
2. When both HI_Z mode and SYSOFF are enable, which mode is preceded?
3. Although the default value of "SYSOFF" is "X", how is this value decided?
Regards,
Kuramochi