We are designing a LiIon battery pack that most likely will be based on the bq40z60. For secondary protection the SLUSAW3C Figure 8 Typical Application Schematic shows a bq294700. This example is for 4 series cells. The associated Note indicates to use bq2945xy for 3s configuaration. The bq2947xy datasheet indicates this part also works for 3 series cell configurations. This part has a external delay capacitor - under what conditions is this external delay required?