Other Parts Discussed in Thread: ISO1540, LM5064
Please tell me about VDD voltage regulation.
According to datasheet, VDD is 4.6V to 5.15V at IDD=0mA, then VDD is 4.8V typ at IDD=-10mA.
Do you have the voltage accuracy data when IDD=-10mA? We would like to know min and max value.
And is it allowed that more than 10mA current flows from VDD? Or should we limit the VDD source current up to 10mA?
We are considering about pull-up resistor of PMBus line with ISO1540. About 15mA(max) is required when pull-up resistor is 1k.
Best Regards,
Kohei Sasaki