those days i am look into LM27403,and here is my question:
1、what is SYNC pin used for ? did the SYNC frequency influence the value of the inductor?
2、in my design,the input voltage is 6-20v, output current is 5A MAX
if i want to dynamicly control the output voltage from 3.0 - 4.5V with 10mv step by mcu,do this application can be realized?
can this be reached by adjust electronical potentiometer of the feedback resistor,and i have seen that when the feedback resistor changes,the error amp component will change.