I am deeply in trouble with TPS61120. It has unique power save features and low power dissipation but I cannot work it out properly.
I have set the output of swmode section to 5.5V and set the LDO section to 5V. Used the design which has given on datasheet Figure 16. After successfully working with the IC at the beginning, after some use, it drops the output voltage to Vin+400mV. Basically it breaks down and never revert back. Switch mode feed back voltage drops to 300mV as well which has to be 500mV according to the datasheet. I think I do damage the IC somehow. What cautions do you advice to protect the IC ? I am careful about ESD and hot plug situations.