This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27421 GPOUT

Hy all


I'm using BQ27421 in one of our devices. The GPOUT pin is unused, but in the datasheet it is recommended to put a 10kOhm Pullup on it. My system should consume as less current as possible (actually I'm around 60uA). With the recommended pullup the current jumps to over  300uA. Is it possible to use a much higher pullup 200 or 500kOhms? Could'nt find some infos about the maximum recommended value.

As I understand the datasheet, GPOUT pin may be an input in HIBERNATE mode. In my System i do not need this mode. Is it possible to let the pullup away?


Thanks for help


Raphael