The TPS544C25 datasheet has an example design and details the CIN and COUT requirements. Page 81 specifies the CIN must be ceramic, although in the example description on pg 82, it states a 100uF polymer cap was also added.
For COUT, no such ceramic requirement is stated, only the ESR MIN must be met. Is there a restriction for COUT to be ceramic, or can TANT/ALUM low-ESR capacitors be used? Webench also defaults to ceramic COUT, and all the alternate devices seem to be ceramic, so is only ceramic allowed for COUT?
~Leonard