Hey guys,
i want to monitor a battery with 10 cells.
This 10 cells can either be configured in a 5S2P setup or a 10S1P setup.
The BQ76930 is able to handle up to 10 cells in series and i was wondering if it is able to handle also a 5S2P setup. Still 10 cells but two separate strings with 5 cells in series for each string. If no, is there another opportunity to do something like that?