Hi,
I need a led driver to control an led of around 30 Watts. I' m going to use two TPS92551 en parallel to get my target of the power.
I need to control the luminous flux with a PWM signal. This signal will be an input to the driver led (TPS92551) but I need to isolate this signal because the HW that is in charge of generating this signal has to be isolated from the power supply of the driver led [LED+ / GND]. The power input to driver leds is 48Vdc.
What do you recommend me for this propouse? My idea is to use an optoisolated IC similar to this schematic:
But then I am going to need a regulator to get 5 Volts to feed the Pull-Up resistors from the power input 48 Vdc. What type of power regulator do you recommend me for this purpose? Is this the best way to get my goal?
Thank you so much. Best Regards.