This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMU

Guru 13485 points

Looking for PMU:

Vin=3.3V

Vo1=4.5V/50MA (boost)

Vo2=2.5V/50MA (Buck)

If available: Vo3=-6V/100MA (negative 6V).If not will use additional device/solution