LM2700 performance analysis.xlsxHi,
We have been testing the LM2700EVM for our product feasibility analysis.
The desired input voltage range is 2.2V - 4.6V. The LM2700 is connected to an LED Load with a Forward voltage of 9V and forward current of 210mA (max).
The test circuit we had used for this testing is shown in the attachment. One thing we would like to highlight is the kind of Feedback circuit we had used. The LED load will be connected to an non-inverting Op-Amp circuit (with a gain factor around 21), the output of which will be the actual feedback voltage for the LM2700.
- As per the test data, we had tabulated, you could see the output current of the LM2700 falling down when the input voltage falls below 2.4V or 2.35V. It was also noted that the corresponding input current is getting reduced at such a operating input voltage condition.
- Also the LM270 IC was seen to gradually heat up when we gradually descend the input voltage beyond 2.5V.
Could someone throw more light on the actual rationale behind this behavior of the LM2700?
Thanks,
Santhosh S