Other Parts Discussed in Thread: BQ76PL536A
I'm working with a board containing 3 BQ76PL536A ICs, and recently the part tripped a few errors in the device status and alert registers. The one of most concern to me is the ECC_ERR bit in the ALERT_STATUS register. It's asserted on one of the BQ76 chips in my board, and seems to be a fatal hardware error
Question: Can the BQ76 recover from an ECC_ERR alert? Or does it signify a hardware problem that requires replacement?
The datasheet is not totally clear on whether or not it can be recovered from. It just states: "The device may return erroneous measurement data, and/or fail to detect COV, CUV, or OT faults in this state". I am seeing lower cell voltages on the ones monitored by the part with the ECC_ERR asserted, while the others continue to function just fine.