Hello to all!
I need a trivial answer about the lm317KCT component. How much is the dropout voltage?
I am not an expert and I do not find this value on the datasheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello to all!
I need a trivial answer about the lm317KCT component. How much is the dropout voltage?
I am not an expert and I do not find this value on the datasheet.
Hello Luca,
Welcome to the forums!
Please refer to Section 7.3 Recommended Operating Conditions:
The minimum recommended Input to Output differential is 3 V.
Best,
Michael
Hello Michael, thank you so much for the reply!
You refer to "Input-to-output differential voltage" parameter right? In this case, this value (3V) it refers to the max output current delivery from LM317, right?
If i have an application where the max load current is about 360 mAh, this value is reduced right?
My application is to build a simple power supply for the microcontroller and a few sensors, having a lipo battery (2s, 7.4V and 1500mAh) to feed all components.
The lipo battery voltage is between 8.4 and 6.4 V, in your opinion it's correct to use a LM317 to power supply this circuit?
Hello Luca,
Yes, the 3V differential is recommended to have maximum current draw. The dropout may be able to be lower under lower current conditions, but I can't speak to how much lower the voltage dropout could go.
You say current is 360mAh, can you clarify? mAh is a capacity and not a current draw. If I assume a constant current over an hour for the given 360mAh, then the current draw would be about 0.1mA, is this correct? If this is the case you also must consider the minimum load current to maintain regulation of 3.5mA typical. If the current draw is below this, then the regulator may not regulate properly and the output voltage will begin to increase above its setpoint.
What output voltage are you trying to achieve? You may be able to use the LM317, but I also am not sure if you are hoping for a higher efficiency in which case you may want to consider a step down switching regulator.
Best,
Michael
Hello Michael!
I'm sorry, but i have a refuse, the max load current is about 360 mA e not 360 mAh!
My load is an microcontroller (200mA) + an MPU9150(estimate about 40 mA over all the work conditions) and 6 HC-SR04 (max current of 20mA, 20mA x 6 = 120 mA) so in total i have a max load current of 360 mA. The work voltage for these components is of 5V.
Under this conditions, the LM317 operate correctly if the input voltage is between 8.4 and 7.4 V?
Otherwise can you give me some tips about some component that i can use to supply correctly my circuit?
PS
I am not interested the efficiency of the component
Best Regards
Luca,
Thank you for clarifying.
If the input voltage is 7.4V and you want to get 5V, the LM317 will not be your best option. The LM317 may be able to do it, but I don't have any data to back that up, so I would just go with the datasheet limits and say that it can't since the dropout is 3V.
In order to guarantee that you get your 5V output over the full range of 8.4V down to 7.4V, I would suggest using the UA7805.
This way you don't even need external resistors to set the adjustable voltage output and you have a fixed voltage regulator that just needs input and output capacitors.
I also don't know if you are looking for a specific package, but the TO-220 is pretty standard.
Typically thermals is also something you want to consider with LDOs. Under worst case conditions you will have a 3.4V dropout with 500mA conservatively so that will be about 1.7W, and the TO-220 (KCS In section 7.4 Thermal Information) has Theta JA of 19 so will heat up about 35 degrees or so, and this is fine for this device since 60C is acceptable.
As for your microcontroller, have you considered our MSP430 line. We have a number of Launchpads for easy prototyping and development : http://www.ti.com/ww/en/launchpad/launchpads-msp430.html#tabs
Always happy to help!
Best,
Michael
Hello Luca,
Again, happy to help.
Some regulators require specific capacitor types due to potential instability from ESR, but for this regulator any type of capacitor should be fine as this device is very stable.
Some references:
https://e2e.ti.com/support/power_management/linear_regulators/f/321/p/38166/133505#133505
https://e2e.ti.com/support/power_management/linear_regulators/f/321/p/300811/1048169#1048169
http://www.ti.com/lit/an/snva167a/snva167a.pdf
Best,
Michael