Hello,
I have a question about TPS38600.
Page-18 of the data-sheet "SBVS105D" describes below.
"Cct(nF) = [tDELAY(ms) – 0.5(ms)] × 0.242 (9)"
"Using this equation, a delay time can be set to between 1.4ms to 10s."
Can I set the RESET-DELAY-TIME for 20sec using 4.7uF?
Is the Max-Cct 2.4uF for 10sec?
Please teach me the way of setting the RESET-DELAY-TIME for 20sec, if it is possible.
Regards,
Daisuke