Hi E2E forum
We are designing a charger using the bq24120 IC.
Can the VTSB be supplied externally or must we use the internalle generated supply?
The internally generated TS bias voltage has a 10 % regulation, which is too large for our application.
Is there a region of operation for the bq24120 where we can obtain a more accurate regulation of VTSB?
(Perhaps most of the regulation range is at the thermal or load extremes)
If possible please provide a plot of the TS bias voltage regulation accuracy as a function of its governing parameter.
Kind regards
Kasper